I am curious about the REG103UA-A and its ERROR Flag pin. The datasheet states that it falls low when the expected output voltage is "approximately" 10% (above or below) out of tolerance. However, the datasheet does not state any electrical specifications on this tolerance, given input voltage and temperature. It only states "approximately".
For example, if the ERROR flag falls low when the output is within +/-10% at room temperature, what is it at-40 deg C? Is it +12/-8%? Or something else? And is it truly +/-10% at room temperature?
I am trying to properly characterize this specification, as we are using it to alert the rest of our system when the output voltage is out of tolerance.
Other things that may be pertinent: Input voltage 3.3V (filtered). Adjustable output voltage setto 2.5V.