This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: Post relax Qmax Update question

Part Number: BQ34Z100-G1

Hi,

I would like to know the minimum requirements for a Qmax update after a partial discharge.

My understanding is this:

a) 37% passed charge is required.

b) 0 amps current flowing (or is this quit current?)

c) dV/dt < 4uV/s (or 5 hours)

1. Is this correct?

2. Also, If the current is less than the "DeadBand" setting is this considered 0 Amps?


Regards,

-Tim