Hello,
I was looking for a DC/DC Flyback converter module from TI. I am planning to use it at output of a solar PV panel where the maximum power will be 250 W. The open circuit voltage is around 35 V and the short circuit current is around 7 A. It would be very helpful if anyone could suggest me a converter which I can use for my project.
Best Regards
Mohammad Arifur Rahman