Dear all,
I have a LM5118-Q1 buck boost SMPS with the following basic specifications of project:
Vin: 10V - 30V
Vout: 12V
Iout: 1A
When I insert power with the SMPS loaded with 22R the circuit starts to buzz and the
output become unregulated like the image bellow:
If I do the opposite, that is, I connect the load after the power input is established the problem doesn't appear.
What it can be?
Thanks in advance.
Geraldo Gomes.