This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40200: Is there a spreadsheet for design calculations, or a better explanation for example calculation

Part Number: TPS40200


Is there a spreadsheet for design calculations, or a better explanation for example calculation

In general the equations are given, but the values used is not shown, so it is pretty difficult to follow the calculations

P21 states: the efficiency target is 90% and the output power 8.25 W.
This gives a total power-loss budget of 0.916 W.
Q: How is this calculated?

P22 states: Using the values in this example, the dc power loss is 129 mW.
Q: Where / How is this calculated

P22 states: Psw = 10mW Equation (10)
What is Ipk, tCHON, tCHOFF

P24 states: The minimum output current for this application is specified at 0.125 A.
How is this specified or calculated?

Any help appreciated