This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS544C25: READ_IOUT Error

Part Number: TPS544C25

Dear Sirs,

 

We’re applying TPS544C25 for 12V to 5V design. However, we found the READ_IOUT is out of spec (+-3A) in datasheet.

Please find the test data below. Could you please explain the root cause of this error and how to fix it in detail? Thanks!

 

Test Condition (A)

0

2

4

6

8

10

12

14

16

18

Actual Load (A)

0

2.008

4.003

6.009

8.002

10.012

12.003

14.013

16.008

18.016

READ_IOUT (A)

0.25

2.63

5.25

7.94

10.63

13.38

16.19

18.75

21.69

24.56

ERROR (A)

0.25

0.622

1.247

1.931

2.628

3.368

4.187

4.737

5.682

6.544

 

Best regards,

Sam Ting