Part Number: BQ76940
Other Parts Discussed in Thread: BQ76930
Dear All:
I am using the BQ76940 to design the 13S BMS ,can you answer the following questions?
1: If connect 13S cells, only need to short VC14 and VC13,VC9 and VC8(BQ76940),C14 and C13,C9
and C8(cell), Do you need an external circuit?
2: External balance use P-FET or N-FET, which one is best?
3:If external balance use P-FET, What is the principle of circuit design? What's the current flow?
4: 16 bit CC: Output value from BQ76940 is 16-bit 2’s Complement Value, then get voltage by CC Reading (in μV) = [16-bit 2’s Complement Value] × (8.44 μV/LSB) by the host ,then get current by divided by the sense resistor, Is that correct? BQ76940 has the fuction of Coulomb calculations?
5: Battery voltage measurement requires 8 cycles ( 2 s), Is it for the average of every cell voltage?
6: The document of " Embedded Scheduler in Cell Battery Monitor of the bq769x0",refer to " Scheduler in Stacking Interface" is bq769x0 daisy-chained?
7: The document of " bq769x0 Family Top 10 Design Considerations", refer to" The more cells are balanced, the more time will be required for the filter to settle", How to understand?
" Balancing every other cell in a group will double the voltage on the unbalanced cell and is typically OK", How to understand? "A FET with a defined RDS(ON) at approximately ½ the cell voltage is desired", How to understand?