Other Parts Discussed in Thread: LM5576, LM5575, LM5161, LM5017, LM5006, LM5145
Hi,
i already have a TPS54160 converter in use to create +6V and -6V from +48V. The Design is similar to the one mentioned in the Application Report SLVA369A. We are really happy with this but now I want to create +18V and -18V from +48V and this exceeds the absolute maximum voltage of the TPS54160 (60V). Does someone have an alternative part for me with an absolute maximum input voltage of >75V?!
Thanks in advance
Florian