This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC2825: UC2825 question

Part Number: UC2825

hello.

I have a question about UC2825.

①UC2825DW
About TJ of UC 2825 DW
Please let me know Tj (MAX).
The maximum value of Tj is not indicated in the data sheet.
Ta = max: 85℃
Power Dissipation = 1 W
θja = 50 ℃ / W
From this, I understand 125℃ is correct, is not it?
② Please tell me how to calculate the loss of UC2585DW.
Do you have this application note?

thank you.