SwitcherPro V3.17 calculates very different values for L and C than the Datasheet example P35
Vin: 18V to 52V, Vout=16V @ 1A
L1=100uH, C2 = 22uF
Datasheet P35 Example:
L1 = 220uH, C9 = 330uF
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
SwitcherPro V3.17 calculates very different values for L and C than the Datasheet example P35
Vin: 18V to 52V, Vout=16V @ 1A
L1=100uH, C2 = 22uF
Datasheet P35 Example:
L1 = 220uH, C9 = 330uF
llo,
Im not familiar with SwitcherPro software you are using.
For calculation purposes use application note
There is also simple spreadsheet for basic calculations for buck regulator
Regards
Brani