This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD3138: HSFB Converter firmware description

Part Number: UCD3138

I have the EVM UCD3138HSFBEVM-029.  I am looking for details about the firmware.    Both the data sheet for the UCD3138 and the EVM user manual state that there is a detailed description of the HSFB converter firmware.    I would like to get that detailed description.    Where can I get it?

  • FYI     reference the following from paragraph 7.1 of UCD3138 data sheet.

    Application Information
    The UCD3138x has an extensive set of fully-programmable, high-performance peripherals that make it
    suitable for a wide range of power supply applications. In order to make the part easier to use, TI has
    prepared an extensive set of materials to demonstrate the features of the device for several key
    applications. In each case the following items are available:
    1. Full featured EVM hardware that demonstrates classic power supply functionality.
    2. An EVM user guide that contains schematics, bill-of-materials, layout guidance and test data
    showcasing the performance and features of the device and the hardware.
    3. A firmware programmers manual that provides a step-by-step walk through of the code.

  • The Technical reference manual is the closest thing that I know of ,and can be downloaded at:
    www.ti.com/.../sniu028a.pdf
    Also, there is a firmware description chapter inside the EVM's user guide.
    If you have any specific questions regarding the firmware please let us know.
  • I have the technical reference manual. I will followup with specific questions as they arise. Thank You