This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP3878-ADJ: Is Vout=1.0v supported, and if so then how?

Part Number: LP3878-ADJ

On the surface, my question seems simple.  But I assure you that it isn't!  :)

On the first page of the datasheet it says, "Output Voltage Range:  1 V to 5.5 V".   But in 8.1 it says, "The LP3878-ADJ can provide 800-mA output current with 2.5-V to 6-V output voltage."  I know, literally the previous paragraph says, paraphrased, "any info below this may be horribly wrong", but still...

So which is it?  I assume that because Vadj=1.0v then min Vout is also 1.0v.  But since the datasheet contradicts itself I had to ask.  So assuming it does Vout=1.0v then I have some more questions.

What about the feedback resistors?  R2 should be a very high value (or maybe missing entirely).  But paragraph 8.1 says R2 should be 1K to 5K.  Given that, R1 needs to be almost 0 ohms.  And if R1=0 then Cff is basically shorted and does nothing.   But again, paragraph 8.1 says that Cff is required to...ensure loop stability.  

Ugg!  What to do?

If it matters, here is what I'm trying to do:  Vin=3.3, Vout=1.0, Iout=5 mA to 300 mA.

Thanks in advance!

  • Hi David,

    Sorry for the confusion on the datasheet. Section 8.1, the correct sentence should be "The LP3878-ADJ can provide 800-mA output current with 1-V to 5.5-V output voltage. " I have put this into our datasheet revision list and it will be fixed on our next datasheet revision. Thanks for pointing this out.

    If you plan to use Vout=1.0V, you don't need to have R2, you can short Vout to ADJ. Cff is also not necessary. We will also fix the section 8.1 in our next datasheet revision.

    Regards,
    Jason Song
  • Hi David,

    Since you want to operate the LDO in unity gain configuration (Vout = Vadj), I recommend R1 = 0. Do not populate R2 or Cff. The lowest output voltage possible with an LDO is generally the Vadj or Vref for the part, in this case 1.0 V.

    In general, a capacitor is not required on a Bypass or Noise Reduction (NR) pin for stability. Also, a Feed-forward cap (Cff) is usually not required for stability. The R2 resistor in the feedback divider usually does not affect stability either.

    I'm adding this datasheet to our list to update/correct. Sorry for confusion caused by inconsistencies and overuse of references to stability.