Hi team
may I get your reply ?
[1] TPS4H160-Q1 A-Version don't have CS pin,
so A-Version cannot detect Open load at On-State ?
if customer wants to detect Open load at On-State,
he has to use B-Version with CS pin output and he has to judge Open load at On-State manually using CS output ?
[2] both A-version and B-version have ability to detect Open load at Off-stage,
but customer needs external pull up resistance for seamless detection ?
[3] D/S recommends 20Kohm external pull up.
BTW,,, what is the Max allowable external pull up resistance to minimize leakage current at Off-stage ?