Other Parts Discussed in Thread: TPS92075
Hi
My customer have a new project need the solution request: 3 step tunable CCT driver solution. other parameter request as below.
1. input voltage: AC120V
2. freqency:47~63Hz
3. output current: 330mA or 200mA
4. output voltage: 36V or 60V
5. output power: 12W
6. current accuracy: 5%
7. efficiecny: >85%
Does we have suitable solution can suggest ? thanks
Jonas zhang