This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR16006: What is value of operating quiescent current (non-switching)?

Part Number: LMR16006


Dear TI,

In the datasheet statement  (Operating quiescent  current (non-switching))  Iq=28uA(typ) 

1. What is the maximum value of Iq?

2. Is the test performed using LMR16006X (Fosc=700KHz) or LMR16006Y(2.1MHz)?

3. If the above answer is LMR16006Y, then LMR16006X Iq=? (Typ/ Max) ?

thanks & Best regards,

Ronald