Other Parts Discussed in Thread: LM2592HV
Hi
I have used 7499210124A as a RJ45 connector and I need to convert the POE voltage to 3.3 volt, so I have some questions:
1- Is it necessary to use TPS2375 or can I connect the POE voltage directly to the LM2592HV?
2- can I connect the 7499210124A RJ45 connector directly to the TPS2375 or I should use DF01S? (there is bridge rectifires in the selected RJ45)
3- is it possible to connect the TPS2375 output voltage to LM2592HV for converting POE voltage to 3.3 volt?
Thank you in advance for guiding me