Datasheet does not specify if pin 3 is internal connected to bottom pad. If not internally bonded connected what of MAX current between pin 3/pad not being listed in AMR? What is the resistance pin 3 to bottom pad also not listed in AMR? Have to ask that question as it requires laboratory grade DMM to measure that low of resistance, if any.
Condition: Bottom pad has PCB bottom foil VIA's route analog ground and top foil digital ground path pin 3. That is to say top foil digital ground is partially isolated from bottom side analog ground via strategically place 20mohm ferrite. DMM indicates 4.4mv drop across grounds isolation ferrite thus indicates 220ma of LDO 3v3 current flow sourced from +5vdc feeding LDO pins 4/6.
Can we assume the two grounds bond inside the TPS pin 3 using two placed VIA of the VSON6 bottom pad? If pin 3 to pad is not bonded on the die perhaps bottom pad did not join in reflow?