Other Parts Discussed in Thread: TPS61253A, TPS61099
Hello,
I am planning to use the TPS61089 for stepping-up voltage of a single Li-ion cell (3V from to 4.2V input range) to 5V.
The load current fall under 500mA, which I feel would be the light load condition for TPS61089 as its Iout is 2A.
In the design created using WEBENCH, the efficiency curves were upward of 85% at around 100mA load,
that efficiency is acceptable for me.
I have only few questions;
Q1. Dose the TPS61089 runs efficiently at light load conditions?
Q2. If not, what could be suitable replacement boost converter with higher efficiency at light load operation?
Thanks and regards!