This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV62568: Operating efficiency at light load conditions?

Part Number: TLV62568
Other Parts Discussed in Thread: TPS62082

Hello,

I am planning to use the TLV62568 for stepping down voltage from 5V to 3.3V.

My load current fall under 500mA, which I feel would be the light load conditions for TLV62568 as its Iout is 1A.

In the design created using WEBENCH, the efficiency curves were upward of 85%

that efficiency is acceptable for me.

I have only few questions;

Q1. Dose the TLV62568 runs efficiently at light load conditions?

Q2. If not, what could be suitable replacement boost converter with higher efficiency at light load operation?

Q3. TPS62082 in WEBENCH design showed better light load efficiency, is it more suitable that TLV62568?

Thanks and regards!