Part Number: BQ2980
Hello,
I am planning to employ BQ2980 as BMS for a single cell Li-ion system.
In the data sheet of BQ2980, under section "5 Device Configuration Options"
for various parts number the UVP (V) ranges from 2.6V to 2.75V.
I don't want my Li-ion cell to discharge below 3V, I want to set the Under
voltage Protection threshold to 3V.
Q1. Is it possible to set a different UVP (V)? If yes the how?
Q2. If not then is there any way to solve this problem?
Thanks and regards