This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS68470GUI: GUI doesn't run under Windows 10

Part Number: TPS68470GUI
Other Parts Discussed in Thread: TPS68470, IPG-UI, USB2ANY

While trying to run the GUI for TPS68470EVM installed on Windows 10 it doesn't run and suddenly windows send a error message:

TPS68470 EVM has stopped working

A problem caused the program to stop working correctly.

Windows will close the program and notify you if a solution is available.

GUI program has been installed on 2 different computers with windows 10 and obtained same results. Even running windows troubleshooting for compatibility issues but no luck. Any suggestions?

  • Hi Manuel,

    If you have a USB2ANY, the IPG-UI can also be used to interface with the EVM. The default project in the IPG-UI is locked, but I can send you a device definition file that should help with your evaluation.

    The compatibility issues with the standalone GUI are currently unresolved.

    Best Regards,

    Rick S.