This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8860-Q1: EEPROM read and write sequence

Part Number: LP8860-Q1


Hello, team

EEPROM writing may fail.
SPI communication mode is selected.

The procedure is as follows
1. Power on
2. VDDIO / EN = LOW
3. Wait 500 μs
4. VDDIO / EN = HIGH
5. Wait 100 ms (SOFT_START = 50 ms + BOOT_START = 50 ms)
6. Write 0x08 to address 0x1A
7. Write 0xBA to address 0x1A
8. Write 0xEF to address 0x1A
9. Write 0x01 to address 0x19
10. Wait 1 ms
11. Write 0x00 to address 0x19
12. Read data from EEPROM registers (address 0x60 ... 0x78).
13. Write 0x08 to address 0x1A
14. Write 0xBA to address 0x1A
15. Write 0xEF to address 0x1A
16. Wait 5 ms
17. Write data to EEPROM registers (address 0x60 ... 0x78).
18. Write 0x02 to address 0x19
19. Wait 250 ms
20. Write 0x00 to address 0x19

After that, when resetting the host microcomputer in the power supply state (starting from step 2), the writing will succeed.
Once again, the host microcomputer is reset (starting from step 2), the writing will succeed.


So I tried various experiments.
Then it turned out that if you set the EEPROM to the locked state after read / write as shown below, the write will not fail.

1. Power on
2. VDDIO / EN = LOW
3. Wait 500 μs
4. VDDIO / EN = HIGH
5. Wait 100 ms (SOFT_START = 50 ms + BOOT_START = 50 ms)
6. Write 0x08 to address 0x1A
7. Write 0xBA to address 0x1A
8. Write 0xEF to address 0x1A
9. Write 0x01 to address 0x19
10. Wait 1 ms
11. Write 0x00 to address 0x19
* 12. Write 0x00 to address 0x1A
13. Read data from EEPROM registers (address 0x60 ... 0x78).
14. Write 0x08 to address 0x1A
15. Write 0xBA to address 0x1A
16. Write 0xEF to address 0x1A
17. Wait 5ms
18. Write data to EEPROM registers (address 0x60 ... 0x78).
19. Write 0x02 to address 0x19
20. Wait 250 ms
21. Write 0x00 to address 0x19
* 22. Write 0x00 to address 0x1A

After unlocking the EEPROM register, is it correct use to lock again?

thanks

  • Hi,

    Unlocking EEPROM twice or locking EEPROM will lock wire access to EEPROM registers, and locking EEPROM after EEPROM programming by writing lock code, unlocking one more time, or cycling VDD will be good to protect programmed EEPROM contents.

    From the first sequence, you're unlocking twice, so EEPROM write won't work.

    From second sequence, you locked before another unlocking, so EEPROM write will work correctly.

    Hope this helps,

  • Hi Sung

    That kind of specification was there.
    Thank you very much.
    Extremely helpful !