This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z60: Problem using emergency Shutdown and Pre-charge features at the same time.

Part Number: BQ40Z60


We have a design where we are controlling the battery Precharge FETs via PIN 14 (GPIO 0) and are using Pin15 (GPIO1) for Emergency Shutdown. It seems that these features are mutually exclusive since precharge will not work if  ESHUT_EN == 1, according to the datasheet: "Pin 14 can be used to control an external circuit for precharge when NR is 1, ESHUT_EN is 0".

How can it be possible that these two features are mutually exclusive of each other? Is there no workaround for this? We have already designed our hardware.

Thanks in advance for your help.