Other Parts Discussed in Thread: LP8860-Q1
Dear, All
I have a question about how to use LP8863-Q1.
I want to suggest with 2ch pair because the current is large from customer's specifications.
In this case, the number of Ch is insufficient in LP8863-Q1.
For this reason we are considering a two-device configuration.
However, for LEDs, turn on only one channel at a time.
For that reason, I would like to share a buck-boost power supply.
question 1:
Since there is a mode in which the LP8863-Q1 uses an external power supply, can this power supply be shared by another LP8863-Q1 the buck-boost power supply circuit?
This configuration is better if it can be used in pairs of LP8863-Q1 and LP8860-Q1.
Question 2:
Is it possible to use LP8863-Q1 and LP8860-Q1 pair using the buck-boost power supply of LP8863-Q1?
Thanks, Masami M.