This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61193-Q1: shorted LED fault behavior

Part Number: TPS61193-Q1


Dear all,

I think below. Is this correct?

If I use LED that has Vf=3V, the shorted LED fault cannot detect when one LED is broken.

I think this because...

at typical condition, LOW_COMP = 0.64V, MID_COMP = 1.64V and HIGH_COMP = 6V,

there are 4.36V between MID_COMP and HIGH_COMP,

so one LED broken (3V) cannnot be detected.

Best regards,