This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Looking for a triple output PCB mount DC/DC converter



Hello

We are looking for a PCB mount DC/DC converter with triple output for a telecom product that will be installed in telecom networks and need help to work out the best option. 

We require a device with the following specs. 

Input voltage range: -36 to -72VDC

Output Voltages: 5.5VDC; 3.3VDC and 12VDC

Maximum rating: About 10-12W

Operating temperature: -40 to +85degC

RoHS compliant

Thanks & regards