Dear Team,
my customer uses TPS40200 and wants to synchronize the device to an external clock.
The datasheet specifies the following requirement:
The maximum amount of time that the RC pin should be held low is 50% of a nominal output pulse, or 10% of the period of the synchronization frequency
whichever is less.“
Can you please clarify what "nominal output pulse" means exactly?
Thanks and best regards,
Joe