This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24266: Enabling output from battery to SYS

Part Number: BQ24266


I’m turning a very quick design for a PCB and I do not have time to test the functionality of the BQ24266 using an eval board. So I’m hoping you can answer a question for me before we have 100 boards made here very shortly.

 

We are using the BQ24266 as recommended, but it’s a requirement to have a high-side FET switch between the battery and the battery input to the charger. See attached snippet.

  Here are my questions:

 

  1. Will the battery still charge when the FET switch is OPEN? I’m concerned with how the IC knows how to charge. Is it putting out a constant float voltage and then looking at the battery current? Or does it need to see a battery voltage before it will charge?
  2. Will the battery still charge when the FET switch is CLOSED? I’m 99% sure it will but I could really use a blessing from someone at TI as this would be a major failure
  3. Looking through the datasheet, I don’t see any ability to disconnect the battery from SYS, even in high-impedance mode. Is this correct?
  • Hi Danny,

    Regarding 1, when charging, you can think of the BAT pin as the output of constant current source with output voltage clamped to the BATREG voltage (4.2V). When OPEN, your FET still has a body diode that will allow current to flow to the battery.

    Regarding 2, no issues, except possible longer termination time due to the added series Rdson of the FET.

    Regarding 3, you are correct. There is no way to turn off the BATFET even in HiZ mode.