Other Parts Discussed in Thread: TPS53317A
1. TPS51200 part can source up to 4.5A max and sink up to 5.5A max (mentioned in datasheet spec). But in TI site it is mentioned as
3A Sink/Source DDR Termination Regulator w/ VTTREF Buffered Reference for DDR2, DDR3, DDR3L and DDR4 |
can you please confirm if it can support 4.5A and 5.5A max?
2. our requirement is to power 10*DDR3 ICs. so there are 14 address lines,6command lines and 3 control lines=28 lines in total. 12mA for sourcing and 13mA for sinking.
for one IC, VTT current =28*13= 0.35A
If same memory controller is connecting channel A to 5*DDR3 SDRAM and Channel B to another 5 DDR3 SDRAM where address, command and control lines are common, how the source and sink current will get affected here? will it be For 10 IC, Current is 3.5A ?
Kindly revert at the earliest.
Thanks and Regards,
Vidhya