Hi All,
Now I have switched to BQ24650, I have two batteries each of 12V in series, So following points are my requirement
1) Lead acid battery of 24V contains 12 Cells
2) Input Vtg. to charge Lead acid battery is 28V DC
3) Charging current required 2.5A
4) Operating temp. -40C to +125C
So I need confirmation on above parameter ( specifically point 1) that BQ24560 will suite perfectly for the application , In addition to that is thermistor compulsory to use???.
Any help will be appreciated!!!
Prashant