This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22810: Any concern if there is GND via on center pad?

Part Number: TPS22810


Hi,

I would like to know whether there is a concern if there is a GND via put on center pad in the layout of TPS22810DRVR (WSON package). Any performance or heat dissipation issue will happen due to this?

TPS22810 is used as load switch where Vin=VBus (5V) with load current of 1A.

Thanks.

Best regards,

Gim Song