My customer is experiencing issues with ripple when the TPS562200 is operating in ECO mode. We have already optimized the ripple with a feedforward capacitor. The intent is to reduce the current in which the device transitions to ECO mode to below 70mA or so. This can be achieved - and already experimented - by increasing the inductor. For 70mA, a 33uH is the calculated value, but the customer ran tests with 15uH and saw significant improvement.
What are the risks of using a 15uH or 33uH inductor in the design?
These are the parameters:
Max Vin = 15V
Vout = 5V
Iout = from 50mA to 1.8A
Max Temperature = 85°C
I appreciate the help!