Other Parts Discussed in Thread: TPS61222, TPS61220, TPS61240
Hello, I'm using the TPS6120 which will be powered by a 3.7V LiPo battery and I want a constant (not adjustable!) output of 5V to power an ATmega32U4. In the datasheet, it establishes that the maximum output current for a Vout of 5V is 600mA and I don't want the uC to be fried. It says that the output current depends on the input to output voltage Down Conversion Mode ratio which I didn't understand very well, and I want to know how can I calculate for R1 and R2 for an output current of maximum 25mA with constant 5V.
In addition, if I want a constant output voltage, would R1 be 0 ohms? If this is true, how would I calculate the value of R2?