This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Requirements Description:
1, a total of 7-way power supply, the current is not particularly accurate, the deviation is not big
2, the key is to find can detect clkreq this signal (pmic Gpio have this function is also the same), detection of this signal if the high level, first to 2v7_nand and 1v8_nand 1v8 Other turn off, continue to detect high level duration of more than 5S (5s10s all line), To turn 1v8_dram and 1v2_dram off. Power is turned on when low level is detected
3, other normal pmic functions, such as supporting the IIC interface, such as the support of OTP functions, such as overcurrent protection, over-voltage protection, resistance to current and voltage impact, such as general functions.
Need to have 2nd special needs
Hi Chao,
You may want to check the LP8758-E0 which is a buck converter, has 4 rails: 1V/4A, 1.2V/4A, 1.8V/4A and 2.5V/4A (by power on default); With 3 load switches, I2C commands, and I2C host GPO or, other timing circuits, it may meet your power need. BTW, for PMIC searching, your Vin specs is also very important.
Please let's know if you have questions.
Thanks!
Phil Yi
Hi Chao,
We don't have exact PMIC for what you mentioned. Please consider my proposal and let me know if you have questions.
Thanks!
Phil