Tool/software: Code Composer Studio
Hi, Im using a single ended BQ76Pl455A-Q1 with the TMS570 microcontroller, I've got the example code loaded in CCS and was just wondering is it possible to set how long balancing is done for at a time, as so far in reading the code I cannot see anywhere that enables the EQn pins. Ideally I'd like to program it so that balancing is done for 0.5s then the voltages are read, repeating until balanced. Is it possible to modify the example code to do this?
Thanks,
Alex