Dear TI,
The problem is that TPS63030 converter is not responding to ENABLE signal if we want to turn off device. Some devices get this after a few on-off cycles, but usually device can work correctly many weeks. During this time converter is enabled and disabled from tens to hundreds, sometimes thousands times. One time it just stucks in ON state and draws the battery to empty in a week. Approximately 10% of devices are affected by this issue.
After it stuck there is no reaction to state changes on ENABLE pin. The only way to turn it off is to completly remove power from device and apply it again. Usually, after first stuck, device stucks every time it is enabled. Some devices goes to completely unregulated state, giving 6.4V output (no matter the input) just after it is powered. Only a few devices after first stuck and power off/on recovery enters normal operation.
Design details
Both schematic and layout are very close to reference. Only difference is additional 100R resistor between VIN and VINA and 2p2 capacitor in parallel to upper resistor in feedback divider. Load is GSM module with 0.14F supercap in parallel.
Vin: 3,3 - 3,6V
Vout: 3,8V
Iin: avg 80mA, 700mA peak (peaks are 577us long with 4.615ms period during GSM transmit burst).
The only untypical thing that we do using IC is supercap charging procedure. If it is empty we are switching regulator ON/OFF using ENABLE pin to not allow battery current to reach more than approx. 0,5A. At the fastest stage device is 1ms ON / 8ms OFF.
Here are input current profiles (200mA/div):
Thank you in advance for your help.
Best regards,
Marcin