This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM27762: The inrush current of LM27762

Part Number: LM27762


Hi

My customer simulated LM27762 the following conditions.
But the input inrush current is 2.3A.
I simulated this device adding the resister on VIN, but I couldn't reduce the inrush current.
Are there there the method to reduce this inrush current?

 Positve:Vin=3.3V, Vout=+2.5V
 Negative:Vin=3.3V, Vout=‐2.5V

Best regards,
Yokota