Other Parts Discussed in Thread: BQ25896, BQ25606, BQ25600
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Andre,
bq24266 and bq25606 were designed to be stand-alone chargers that do not require a host u-controller. The bq25600 and bq25896 will operate in default mode without a host processor but you cannot change charge current and some other default settings without a host u-controller.
Hi Andre,
Normally, you can estimate the necessary input current from the desired using the datasheet efficiency curves but this datasheet only shows data for VIN=5V. I suggest you look at the host controlled version, bq24261, datasheet page 11 figure 2. Then use efficiency = VBAT*IBAT/(VIN*IIN) to compute IIN. For example, for IBAT=3A and VIN=5V, you will need slightly more than IIN=3A.
)