This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5160-Q1: Inductor value of PMP10733

Part Number: LM5160-Q1
Other Parts Discussed in Thread: PMP10733, LM5160

Hi,

We got a question from the customer about LM5160-Q1.
Could you help us?

[Question]
They are considering using LM5160-Q1 for Fly-buck-boost topology under the following condition.

 Vin=8V to 16V
 Vo_pri=15.4V
 Io_pri=0A
 Vo_sec=15V
 Io_sec=500mA
 fsw=200kHz

They found PMP10733 which is close to their requirement. So they have question.

22uH couplead inductor is used in this design and it makes big inductor ripple. Why is 22uH used in this design?

They are considering using 68uH to 100uH for thier requirement. Because if the small inductance such as 22uH is used, the inductor current reaches the current limit. Is there any concerns about using 68uH to 100uH inductor for thier design?

Best Regards,
tateo