This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Part suggestion for VVDN

Other Parts Discussed in Thread: BQ24630, BQ24105-Q1

Hi Ti Team,

We planned to use Battery powered system in one of our project, for that we seeking an perfect battery charger IC with all our below criteria satisfied.

Battery Specificaiton:

Chemistry Type: LiFePO4 (Lithium Iron Phosphate)

No. of series Cells: 2

Battery Output Voltage: 6.4V

Capacity: 850mAH to 1000mAH

Charger IC Requirement:

Must be Automotive Grade part (AEC-Q100)

Must be Switching Buck converter with Integrated Mosfet

Must support min of 2 series cell charging.

Control Interface must be Stand Alone type.

Input/supply voltage: 12V

Please help here to find out suitable battery charger IC part number and let us know if any clarification needed.

  • bq24630 can meet the requirement except "Must be Automotive Grade part (AEC-Q100)".
    The only multi-cell automotive Grade part (AEC-Q100)" that I know is bq24105-Q1 which is a Li-ion battery charger: the charge voltage setting is flexible which can support 2S LiFePO4 battery charge voltage. But, the re-charge threshold, pre-charge threshold and TS pin setting are different than LiFePO4 setting.