I want to use the bqStudio to generate a chart recording the data in the whole process of learning cycle.
But it seems that the bqSdudio can only record about 2000 points.
When data points goes beyond 2000,the curve move to the right slowly. the data in the beginning is lost.
I try to change the auto scale threshold. I also try to disable the auto scale function and set the maximum scale to 129600.
The results are the same, the curve slowly move to the right and I get a curve with only about 2000 data.
How can I do to abtain a curve recording data for a long time?