Hello, BQ27750EVM with connected battery and programed flash was tested and work OK, but after some time "unoccupied" when I try to conneckt again - the I2C communication is not start and FET is not control, looks like the microcontroller is frozen becouse voltage was OK (more than under voltage therhold).
I connected charger, hope activeted, but it was not help. Also charge current is not start. I recover BQ27750 only after disconnet/connect battery cell. My question: How can I reset BQ27750 without disconnet/connect battery cell? Is there WDT or somethig like this?
Thank you. Best regards, Danil