This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AC/DC converter for 230V/50Hz and 115/60Hz

Prodigy 130 points


Hello Support Team,

Please propose the solution for designing AC/DC conveter from 230V/50Hz. 

115/60Hz grid is optional. It must be foreseen in the design in such way that with a minimum of component changes the CU can be used for 115/60Hz. 

Required output voltages are 24 VDC, 5 VDC, 3V3 @4A