Hi all
My customer is working on a design with the TPS561201, specs are:
12V => 3.9V/0.5A
In their application they have an output load capacitor of up to 200uF, this is definitely higher than the recommended Datasheet value.
They have these questions:
Is it ok to use an output capacitor of 120uF ... 200uF with the TPS561201 ?
If yes: What inductor value should they choose ?
The Datasheet recommends the LC-frequency should be below the "high frequency zero"
Please provide a value for the "high frequency zero"
Best regards
Ue