This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53353: Bench test report for Vout=0.9V condition

Part Number: TPS53353

Hi There:

I'd like to based on the TPS53353EVM-744 this design to change the output into 0.9V and double check the efficiency performance for customer.

Do we have the test result already done when Vout=0.9V / Full load= 20A? 

Reference from Webench result, it's known the eff could be from 63% to 87.5% around. (set Vin=12V)

But do we have the result for the scope of current from 0.1A or 0.5A? It would be much clear for customer to check the eff performance for any specific loading