Other Parts Discussed in Thread: UCC27714
Hi,
I am going to use UCC256302 as an half bridge LLC regulator for converting 320V to 50V @ 40A.
1.In UCC256302 datasheet Page no:14,It is mentioned as that the internal driver can drive LLC power stage upto 500W continuous power.
Shall I use external gate driver for higher drive current for my mosfet?If drive current is an issue.
2.Is there any provision to fix the minimum switching frequency of regulator IC to 650Khz in order to avoid the transformer saturation.