Other Parts Discussed in Thread: LM5010
Hi,
Because R&D needed wide input range DC-DC converter, R&D refereed to the application note AN-1352(snva101a).
On this document, there is a example input voltage range 12V to 75V.
On the data sheet, the input voltage absolute maximum rating(VIN) is 75V.
Customer input rage is up to 72V.
Is LM5010 suitable for the application wide input range up to 72V?