This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5085: Buck Controller duty cycle and output current queries

Part Number: LM5085
Other Parts Discussed in Thread: LM5145

Hi Team 

We are planning to use LM5085 Buck regulator in our design and we are having queries which are as below:

1) If input will be Vin<= 12V then what will be the output of LM5085 and whether that voltage will be stable or not as MP1498 has wide i/p range (4.4V- 60V)?

2) We need 60W output (system requirement) from LM5085 which means (12V/5A) or (10V/6A).Can LM5085 provide 6A to load at 10V? If yes then how can we choose PFET used in that circuit?

3) In LM5085 , external Mosfet is there which is taking more space. Is TI having any parts which work in 100% duty cycle same as LM5085 but inbuilt MOSFET? 

For the better understanding image is attached below.

Looking forward to your valuable response.