hi all
a customer of mine is testing TPS62088 EVM.
They observed 2 failures of the TPS62088 device, so far:
1.) The first TPS62088 device failed under "no load test" and the input voltage was increasing from 3 to 4 V.
2.) The second TPS62088 device failed under "light load test (Rout = 7 Ohm)" and the input voltage was increasing from 3 to 4 V.
The input voltage was powered from a programmable DC power supply with the current limit set to 400-600 mA, and voltage was swept from 2.5 V - 4.5 V.
The TPS62088 EVM board was used with jumpers at default positions.
any hint?
thanks a lot in advance
KR
Vincenzo