Other Parts Discussed in Thread: LMS3655, LM73605,
Hi there,
Do we have any device (or any roadmap devices) similar to XR76205?
It has to be a converter with synchronous rectification.
Thanks!
Best regards,
Roy Hsu
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
LMS3655 or LM73605 is 5A synchronous buck converter. pls check data sheet on TI website and let us know if any more question.
Roy,
I check data sheet and below eff data for your reference:
Vin : 12V / Vout = 5V / Iout = 5A
LMR14050 eff=88% LM73605 eff=92%
Vin : 12V / Vout = 3.3V / Iout = 5A
LMR14050 eff=83% LM73605 eff=90%
high perfromance LM73605 has better conversion eff than LMR14050 which is more cost-effective.